AMI Database Configuration

  1. Modify the following items in the 02_RxAmiViews.sql file before executing the database scripts:

    1. Replace 'US/Mountain' by 'US/Eastern' or appropriate time zone based on server location.

    2. Modify the stale threshold in the section that creates the RXINT_AMI_CALLS_TO_SUBMIT_VW view.

    3. Modify the momentary threshold in the section that creates the LP_HIST_NON_MOMENTARY view. The default value is 1 minute. If an outage is shorter than the set threshold, it is considered a momentary outage.

  2. Open a command prompt and execute the install_AMI.bat script, which is located at:

    For Oracle, the batch script is located in C:\Program Files (x86)\Miner and Miner\Responder\Integration\Ami Service\IntegrationScripts\Oracle

    This script requires the following files, which should be in the same folder:

    1. 01_RxAmiCustomTables.sql

    2. 02a_RxAmiDownEventViews.sql

    3. 02b_RxAmiUpEventViews.sql

    4. 02d_RxAmiTiltViews.sql

    5. 02e_RxAmiCallsViews.sql

    6. 02f_RxAmiRestoresViews.sql

    7. 03_RxAmiIndexes.sql

    8. Ping_Request_Table.sql

    9. RxIntAmiKillSP.sql

    10. RXINT_CONFIGURATION_oracle.sql

    11. Set_RXINT_CONFIG_oracle.sql

    For MS-SQL, the batch script is located in C:\Program Files (x86)\Miner and Miner\Responder\Integration\Ami Service\IntegrationScripts\MS-SQL\

    This script requires the following files, which should be in the same folder:

    1. 01_RxAMICustomTables.sql

    2. 02_RxAmiViews.sql

    3. 03_RxAMIConfiguration.sql

    4. RxIntAmiKillSP.sql

  3. Provide the Responder your username, password, and database instance when prompted. For example:

    User name: responder (or any preconfigured user with database admin rights)

    Password@Instance: password@tnsname

    The batch script runs the SQL scripts to create the necessary database structures for AMI integration.

  4. Execute the install_Archive_AMI.bat script, in the same location.

    This script requires the following files, which should be in the same folder:

    1. 01_RxAmiCustomArchiveTables

  5. Provide the Archive schema username, password, and database instance when prompted. For example:

    User name: rxarchive (or any preconfigured user with database admin rights)

    Password@Instance: rxarchive@tnsname

    The batch script runs the SQL scripts to create the necessary database structures in the archive tables for AMI integration as listed below.

    • Adds the following tables:

      • RXINT_METER_EVENT

      • RXINT_METER_EVENT_HISTORY

      • RXINT_PROCESS_LOGS

      • RXINT_PING_REQUESTS

      • RXINT_PING_REQUEST_METERS

    • Adds the RXINT_CONFIGURATION table and sets the values for those selected during install.

    • Adds the RxInt Ping Meter task and assigns it to the Dispatcher role.

    • Adds the RXINT_AMI_TIME_RESTORED field to the RX_CALLS, RX_CALLS_HISTORY, and RX_CALLS_ARCHIVE tables.

    • Adds the rx_calls_trg trigger to the RX_CALLS table.

    • Adds the following Views:
      • LAST_EVENT_VW

      • RXINT_AMI_DOWN_COUNT_VW

      • RXINT_AMI_DOWN_EBI_VW

      • RXINT_AMI_DOWN_FLAG_VW

      • RXINT_AMI_DOWN_KM_VW

      • RXINT_AMI_DOWN_RATE_VW

      • RXINT_AMI_DOWN_TILT_INTRVL_VW

      • RXINT_AMI_TILT_DOWN_INTRVL_VW

      • RXINT_AMI_TILT_EVNT_VW

      • RXINT_AMI_DWN_EVNT_VW

      • RXINT_AMI_UP_COUNT_VW

      • RXINT_AMI_UP_EBI_VW

      • RXINT_AMI_UP_FLAG_VW

      • RXINT_AMI_UP_KM_VW

      • RXINT_AMI_UP_RATE_VW

      • RXINT_PING_RESPONSES_VW

    • Adds the CheckAmiKillTriggers Stored Procedure.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.