Web Configuration for IVR

The table below shows web.config settings used for optional integration with MultiSpeak.

Config Key

Config Description

Config Value

Ivr.EventMap

To define the event type mapping between the MultiSpeak and Responder.

Ivr.EventMap

Ivr.CallBackStatusMap

To define the Callback status mapping between the MultiSpeak and Responder.

Ivr.CallBackStatusMap

IvrCallRemarks

Remarks that appear for every call created via IVR integration.

Call by IVR

IvrCallRecordId

Field Name of the custom field added by the integration to store the call id in the IVR system. Used when closing the call or while submitting the Callback.

RXINT_CALL_RECORD_ID

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.