SCADA Database Configuration

  1. Open a command prompt and the execute install_Scada.bat script.

    • For Oracle, the batch script is located in:

      C:\Program Files (x86)\Miner and Miner\Responder\Integration\Scada Service\IntegrationScripts\Oracle

    • For MS-SQL, the batch script is located in:

      C:\Program Files (x86)\Miner and Miner\Responder\Integration\Scada Service\IntegrationScripts\MS-SQL.

    This script requires the following files, which should be in the same folder:

    • 01_RxScadaCustomTables.sql

  2. Provide the Responder Username, password, and database instance when prompted to do so. For example:

    User name: responder (or any preconfigured user with DB admin rights)

    Password@Instance: password@tnsname

    The batch script runs the SQL scripts to create the necessary database structures for the SCADA integration as listed below.

    • Adds the following tables:

      • RXINT_SCADA_EVENT

      • RXINT_SCADA_EVENT_PROCESS

      • RXINT_PROCESS_LOGS

      • RXINT_SCADA_EVENT_HISTORY

      • RXINT_SCADA_EVENT_PROCESS_HIST

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.