Web Servers

The following steps should be executed prior to starting installation of the Common Interface Module and MultiSpeak module for RxIF to help make sure your web server is ready for the installation.

  1. Ensure IIS is installed and configured.

  2. Open IIS Manager and create an application pool with the following configuration:

    • Name = SE.Responder.Integration (this is a suggested name, you can name it anything you would like).

    • .Net Framework Version = .Net Framework v4.0 (and later).

    • Managed Pipeline Mode — Integrated

  3. Start the Application pool.

  4. Navigate to the Advanced Settings of the Application and set the following properties:

    • Enable 32 bit Applications = True

    • Identity = ApplicationPoolIdentity

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.