SCADA Configuration Batch Scripts

Execute the Configure_SCADA.bat located in the path C:\Program Files (x86)\Miner and Miner\Responder\Integration\Configuration\Scada

This script must be executed on all machines where RxIF Server has been installed.

This script requires the following files:

  • ScadaDatabaseSchemaConfig.xupdate

TIP: If the installation is an upgrade or patch fix, please save a backup copy of DatabaseSchemaConfig.xml from the C:\Program Files (x86)\Miner and Miner\Responder\Server folder. After the batch script use an XML file compare function to compare the new configurations with the backup configurations and verify changes (Notepad++ or XMLPad).

The files changed by the xupdates are as follows:

  • DatabaseSchemaConfig

    • Adds the Int_Device_Status domain.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.