Service Configuration

Update the application configuration file Miner.Responder.RxIF.CisBatchProcess.exe.config located in C:\Program Files (x86)\Miner and Miner\Responder\Integration\CisSyncApplication or the installed path, if it was changed during installation.

  1. Change the log file location, if required. By default the log file will be placed in C:\Files\CIS\Logs.

    <appender name="RollingLogFileAppender" type="log4net.Appender.RollingFileAppender">
    <param name="File" value="C:\Files\CIS\Logs\RX_CIS.log"/>
    <appender name="MissingRollingLogFileAppender" type="log4net.Appender.RollingFileAppender">
    <param name="File" value="C:\Files\CIS\Logs\RX_CIS_Missing.log"/>

  2. Change the MSMQ ComputerName to the FQDN of the Responder Server.

    Verify that the ComputerName is not populated, it should say ComputerName.

    <wellknown type="Miner.Responder.Shared.IDataServices, Miner.Responder.Shared" url="msmq://FormatName:DIRECT=OS:{ComputerName}\private$\RxServer/DataServices.rem" />

    Set the ComputerName here:

    <channel ref=”msmq” ComputerName="ComputerName" />

  3. Application Configuration

    The tables below provide explanation and examples of service configurations.

    Cis Database:

    Config Key

    Config Description

    Default Config Value

    ServerName

    Database server name.

    For sqlserver, the ServerName setting should contain the server and instance

    Oracle: “minerva.miner.com”

    SQL Server:

    "marlins\mssql5"

    ServerSID

    Database SID.

    For sqlserver, the ServerSID setting should contain the database, e.g. GIS

    Oracle: “minerva.miner.com”

    SQL Server:

    "GIS"

    ServerServiceName

    Service name for Oracle

    “orca9.minerva”

    ServerUser

    Server username

    “responder”

    ServerPass

    Server Pasword

    “responder”

    ServerUseOracle

    If Oracle needs to be used mention true

    false

    ServerUseServiceName

    If Oracle Service Name needs to be used mention true

    false

    Rx Database:

    Config Key

    Config Description

    Default Config Value

    RxServerName

    Rx Database server name.

    For sqlserver, the ServerName setting should contain the server and instance

    Oracle: “minerva.miner.com”

    SQL Server:

    "marlins\mssql5"

    RxServerSID

    Database SID.

    For sqlserver, the ServerSID setting should contain the database, e.g. GIS

    Oracle: “minerva.miner.com”

    SQL Server:

    "Responder"

    RxServerServiceName

    Service name for Oracle

    “orca9.minerva”

    RxServerUser

    Server username

    “responder”

    RxServerPass

    Server Pasword

    “responder”

    RxServerUseOracle

    If Oracle needs to be used mention true

    false

    RxServerUseServiceName

    If Oracle Service Name needs to be used mention true

    false

    SQLString

    Specify the staging view name which contains data from CIS

    "SELECT * FROM RESPONDER.RESPONDER.RX_CUSTOMERS_CIS_VW {0}"

    SetDefaultOID

    Determines whether to set a default service point ObjectID for a customer whose service point cannot be found in GIS.

    false

    DefaultOID

    The default service point ObjectID to assign to customers that cannot be associated with a service point in GIS.

    320212

    ChangeVersion

    Set to true if not using sde.default version searching service points in GIS.

    false

    Version

    Name of version to use for searching for service points. (this is ignored if the above parameter is set to false).

    SDE.DEFAULT

    CustomFields

    A comma-delimited list of custom fields in RxCustomers table to be populated. These field names should also match the names of the corresponding source fields in the staging view referenced in the SQLString parameter above.

    Example:

    TransformerId, LocationId

    ExcludedColumns

    A comma-delimited list of fields in RxCustomers table to exclude from the sync.

    Example:

    FEEDER_ID

    UseSecondaryID

    Determines whether to use an additional field (in addition to ACCOUNT) for searching for matching customer in RxCustomers table. If match is not found by ACCOUNT, then the additional field is searched.

    false

    SecondaryID

    Additional field to use for searching for matching customer in RxCustomers table.

    SID

    LogUpdates

    Determines whether to include detailed logging of individual field updates in the application log file.

    true

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.