AMI Service Configuration

To make the following optional changes, update the configuration file Miner.Responder.RxIF.AmiService.exe.config located in:

C:\Program Files (x86)\Miner and Miner\Responder\Integration\Ami Service (or the installed path, if it was changed during installation).

  1. Change the log file location, if required. By default the log file is placed in C:\Responder\Logs.

    <file value="C:\responder\logs\Miner.Responder.RxIF.AmiService.log" />

  2. Change the MSMQ ComputerName to the FQDN of the Responder Server.

    Verify that the ComputerName is not populated, it should say ComputerName.

    <wellknown type="Miner.Responder.Shared.IDataServices, Miner.Responder.Shared" url="msmq://FormatName:DIRECT=OS:{ComputerName}\private$\RxServer/DataServices.rem" />

    Set the ComputerName here:

    <channel type="Miner.Responder.Shared.Channels.MSMQ.MSMQChannel, Miner.Responder.Shared" ComputerName="ComputerName " responseTimeout="00:06:00" />

  3. Application Configuration

Config Key

Config Description

Default Config Value

Ami.ProcessWaitInterval

Time between two subsequent processing cycles

00:00:30

Ami.StaleEventThreshold

This setting is obsolete. The Stale Event Threshold must be configured in the Web Server. Please see the documentation for the Web Server you are using, either Multispeak or CIM.

02:00:00

Ami.EventPersistDuration

The amount of time to keep the meter events in the RXINT_METER_EVENT table before they are archived to the RXINT_METER_EVENT_HISTORY table.

02:00:00

Ami.ArchivePersistDays

Maximum number of days an event record is kept in the RXINT_METER_EVENT_HISTORY table.

15

Ami.ArchiveInterval

The frequency of running the job responsible for Archive and Delete from Archive.

00:01:00

Ami.ChunkSize

Number of calls submitted per request. Used in conjunction with the number of records retrieved by database view. The two numbers control how many dataservices would the AMI integration require.

500

AMITimeToWait

How far back to look for unrestored meters in seconds.

180

AMIWaitInterval

How often to check for unrestored meters in seconds.

60

CreateNestedOutages

If true, create nested outages for meters that Responder thinks are restored, but have not received a power up from AMI after waiting the AMITimeToWait amount of time

False

NestMode

Determine how to create nested incidents. MultipleIncidents, SingleIncident, or Nest are options for this setting.

MultipleIncidents

NestComment

Text to appear on COMMENTS for the Incidents created as a result of Nested Outage scenario

AMI Nested Incident

CheckResponderRestore

If true, an additional check is done to get a list of meters restored recently. Power downs from those meters are then filtered out. This feature is meant to work in conjunction with the RxIF SCADA integration, so should be turned off if you do not have SCADA

FALSE

Ami.ResponderRestoredThreshold

How far back to check Responder for recently restored meters

0:10:00

EFCommandTimeout

Entity Framework command time-out, in seconds. How long a sql command can run before it times out

300

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.