Web Configuration for AMI Using CIM (optional module)

The table below shows web.config settings used for optional integration with AMI using CIM.

Config Key

Config Description

Config Value

Ami.StaleEventThreshold

Events received after this threshold compared to the system time are considered stale and not processed.

02:00:00

Ami.EventMap

Mapping of AMI Events defined in CIM and required in Responder.

Ami.DefaultEventMap

Ami.PingResponseMap

Mapping of AMI Events defined in CIM and required in Responder.

Ami.DefaultPingResponseMap

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.