AMI Outbound Service (optional module)

Installation Steps – AMI Outbound Service Installation and Configuration

This is an optional module and is not required to run RxIF.

  1. Run the RxIF.AmiOutboundService_####_Release installer. In the Welcome dialog, click Next.
    TIP: The #### in the installer name represents the release number. For example, if you are installing 10.6.1b, the installer name is RxIF.AmiOutboundService_1061b_Release, and the 10.8.1 installer name is RxIF.AmiOutboundService_1081_Release.
  2. Enter the Username and password of a domain or local user that will run the service. It must be a valid Responder user. Then click Next.

  3. Choose a database and click Next.
  4. Enter the credentials for the database and click Next.
  5. Specify the MSMQ Server (eg., localhost, machinename@domain.com) and click Next.
  6. If ArcFM is installed, the same install location will be used. Otherwise ensure that the location is set to C:\Program Files (x86)\Miner and Miner\ or use the Browse button to select it, and click Next.
  7. Start the installation by clicking on the Install Button.
    The installation will complete and the files will be deployed to C:\Program Files (x86)\Miner and Miner\Responder\Integration\Ami Outbound Service.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.