Message Router Servers

This section walks through the installation and configuration of message router servers. These are optional modules and are not required to run RxIF.

Router Server

Another service user may be needed to set up the following routers, called “RxApp,” which will need to be added to the Responder database users. Alternatively, you may add the Responder Service user to the Responder users database.

IMPORTANT: Responder and its Integration Framework's processes are likely to use more resources during large-scale activity. This can affect the performance of other applications running resident scans on inbound and outbound Responder activity. We recommend you add exceptions to such applications for all Responder processes, in a lower environment, analyzing performance impacts and security implications to your business, and promoting up necessary changes. Further consultation can be provided by Schneider Electric.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.