Locate Webservice URL

There are times when you'll need to supply your webservice URL to your SCADA vendor. To find the URL to give to the SCADA vendor, complete the following steps.
  1. Open IIS.
  2. Navigate to Sites\Default Web Site and click on the MultiSpeak node.
  3. For MultiSpeak3.0ab, click on Content View, then right click on OAServer.asmx and choose Browse.

    For MultiSpeak4.1.6, click on Content View, then right click on OAServer.svc and choose Browse.

    This opens the web site in the default browser.

  4. The URL you are looking for is in the Address bar. For example:
    • For MultiSpeak3.0ab: http://localhost/Miner.Responder.RxIF.MultiSpeak30ab/OAServer.asmx

    • For MultiSpeak4.1.6: http://localhost/Miner.Responder.RxIF.MultiSpeak416.Service/OAServer.svc

  5. Replace localhost with the IP address of the server, and then add /basicHttp needs to the end of the URL. For example:
    • For MultiSpeak3.0ab: http://123.456.78.9/Miner.Responder.RxIF.MultiSpeak30ab.Service/OAServer.asmx/basicHttp

    • For MultiSpeak4.1.6: http://123.456.78.9/Miner.Responder.RxIF.MultiSpeak416.Service/OAserver.svc/basicHttp

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.