RxIF Client

To install the Install RxIF Client:
  1. Run the MSI file RxIF.Client_####_Release.msi.
    TIP: The #### in the installer name represents the release number. For example, if you are installing 10.6.1b, the installer name is RxIF.Client_1061b_Release.msi, and the 10.8.1 installer name is RxIF.Client_1081_Release.msi.
  2. In the Wizard dialog, ensure the location is set to C:\Program Files (x86)\Miner and Miner or change it by clicking the Browse button.
  3. Begin the installation by clicking on the Next Button, then the Install button.
  4. The installation will complete and the files will be deployed in the installed path.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.