Apply a View Filter
Available View Filters are accessed by clicking or tapping the funnel icon.
To deliver consistently fast performance, ArcFM Mobile supports View Filters only in offline mode with downloaded data (preferred) or in online mode with locally rendered data. Opening the View Filters pane in online mode without local rendering yields a message that filtering is unavailable.
Switching to offline mode restricts the operational map display to features that have been downloaded for offline use. Once offline, clicking or tapping the funnel icon displays a list of available View Filters. In this example, one filter called FeederID has been defined.
Entering a value in the filter box restricts the displayed features to those matching the filter criteria. In this example, only those features with a Feeder ID of 541 are shown on the map.
You may include more than one filter criterion, separated by commas. In this example, the map displays features with a Feeder ID of 541 or 542.
Normal Search and Identification tools remain available to the user when a View Filter has been applied. In this example, the user applies a lasso tool to identify features.
Because the View Filter has been applied, the features identified here all have a Feeder ID of 541 or 542.