Notifications

Publishes in WPF and Xam and Android {Windows and iPad and Android }

Publishes in all
Notifications provide a history of messages displayed for events, including:

  • Successful Offline Package downloads

  • Unsuccessful Offline Package downloads

  • Unsuccessful attempts to load a map

  • Removal of markup graphics from the map

WPF
Click the Notification  flag to display the Notifications pane. Individual records in the pane can be removed by clicking Dismiss next to the item. Click Dismiss All to clear all records from the pane. To close the pane, either click the X or the flag icon.

WPF
As notifications arrive, the flag appears with an exclamation by it , until you click to dismiss them.

Publishes in all
If there are no notifications, the flag is plain grey with a green background .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?