Zoom In and Out on Map

Publishes in WPF {Windows}

At the bottom right of the map are two zoom buttons:

These buttons are used to zoom in or zoom out on the map.

TIP: You can also zoom in by repeatedly double-clicking in the map.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?