Measure Tool
The measure tool gives you the ability to measure distances in a map in order to estimate locations in the field. The tool is located in the lower right of the app and looks like a small ruler.
This tool pulls units (i.e., meters or feet) directly from the current operational map’s units. Therefore:
-
If the currently selected operational map has a coordinate system that uses the units "esriFeet," then the measurements are always in imperial measurements (feet or miles).
-
If the coordinate system uses "esriMeters" units, then the measurements are always metric (meters or kilometers).
The tool begins to show measurements in miles or kilometers once a distance is long enough. So, if your distance is greater than 1 km, the tool starts showing you kilometers. Likewise, greater than 5,280 ft of distance provides you with measurements in miles.
This is a very handy tool in the event that, for example, you have a fault indicator notifying you how far down a feeder that a fault has occurred.
-
WPFClick to place the first vertex.
-
WPFContinue clicking to place vertices until you reach the desired length, then you can determine the fault location in the map.WPF
Another handy use for this tool is when you need to find a buried switch box in a field.
-
WPFClick to place the first vertex.
-
WPFClick to see the sidewalk measurement.WPF
-
WPFClick again to see the total distance out in the “field.”WPF
-
Use both segment lengths to estimate the switch box’s location so you can access it.