Markups

Markups allow you to place features in the map to be incorporated as appropriate into your GIS system. ArcFM Mobile supports designation of one or more markup types (gas markups vs. electric markups). Markup tools are determined by the feature services that have been configured by your administrator.

Markups can be performed with a mouse, stylus, or finger (depending on your device), and all actions are performed in a similar manner.

Markups placed in the map are saved as you place them, so if the application is closed and reopened, all edits are still displayed in the map.

TIP: If you switch operational maps after placing markups, the markups you placed before switching are there when you switch back.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?