Create and Send Markups
- Click the name of the markup type you need for the current
session.
The following is an example of the markup toolbar, which is defined for the current operational map, that is displayed after tapping Markups with Attributes in the image above:
See Adding Markup to a Map for details on placing different kinds of markups.
- To send the current markups, click the Send
button. Click
Yes or No to send the markups or to abort the send. The markups turn
transparent in the map.TIP: After you click the send button, the markups are automatically sent for review. The markups remain transparent in the map until they are approved and completed in ArcMap or ArcGIS Pro. Once the markups are completed, they are automatically removed from ArcFM Mobile. If your device is offline when you send the session, the app automatically sends the markups once it detects an internet connection. - To view the markups in ArcFM, click the Refresh
button on the ArcFM Markups toolbar then view and/or zoom.