Electric Tracing

To illustrate the use of electric tracing, we are going to perform a trace on a primary conductor.

  1. After selecting the desired Operational Map, zoom/pan to the area of interest.
  2. Click the Isolate button at the bottom of the app to enable it, at which point it turns green, , then click the desired location in the map. A blue circle appears where you clicked.

  3. The results are displayed both in the map and in the Trace pane, which opens automatically if it isn’t already open. Color-coding is based on phasing. The initial view zooms to encompass the entirety of the downstream trace, and the upstream trace to the first protective device. You can zoom as needed to see the full trace.
  4. Click the Clear button in the top right corner of the Trace pane to clear out the results of the current trace.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?