DOCA0091FR-08

Logiciel EcoStruxure Power Commission

Présentation

Info. to experts (09/2016): This map content is present in IFE User Guide, IO Module User Guide, FDM121 User Guide, ULP System User Guide, and also Masterpact NT/NW and Compact NS Modbus Communication Guide, Masterpact NT/NW and PowerPact P- and R-Frame Modbus Communication Guide, Compact NSX 100-630 A Modbus Communication Guide, PowerPact H-, J-, and L-Frame Modbus Communication Guide. Any changes made will be made in all these guides.

@TechPub Writer (10/2016): Variables used in the block “Overview” are shared in maps D-SE-0059996 and D-SE-0052515.

EcoStruxureTM Power Commission est le nouveau nom du logiciel Ecoreach.

EcoStruxure Power Commission software helps you to manage a project as part of testing, commissioning, and maintenance phases of the project life cycle. The innovative features in it provide simple ways to configure, test, and commission the smart electrical devices.

EcoStruxure Power Commission software automatically discovers the smart devices and allows you to add the devices for an easy configuration. You can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Additionally, when the panels are under operation, any change of settings made can be easily identified by a yellow highlighter. This indicates the difference between the project and device values, and hence provides a system consistency during the operation and maintenance phase.

Le logiciel EcoStruxure Power Commission permet de configurer les disjoncteurs, modules et accessoires suivants :

Gammes de disjoncteurs

Modules

Accessoires

Disjoncteurs MasterPact MTZ

  • Unité de contrôle MicroLogic X

  • Modules d'interface de communication : interface IFM, interface IFE, serveur IFE et interface EIFE

  • Modules ULP : Module IO

    , afficheur FDM121*

Module de sortie M2C

  • Disjoncteurs MasterPact NT/NW

  • Disjoncteurs ComPacT NS

  • Disjoncteurs PowerPacT P- and R-frame

  • Déclencheurs MicroLogic

  • Modules d'interface de communication : module BCM, module CCM, module BCM ULP, interface IFM, interface IFE, serveur IFE

  • Modules ULP : module IO, afficheur FDM121*

Modules de sortie M2C et M6C

  • Disjoncteurs ComPacT NSX

  • Disjoncteurs PowerPacT H-, J- and L-frame

  • Déclencheurs MicroLogic

  • Modules d'interface de communication : module BSCM, interface IFM, interface IFE, serveur IFE

  • Modules ULP : Module IO, afficheur FDM121*

Modules de sortie SDTAM et SDx

Pour plus d'informations, reportez-vous à l'aide en ligne du logiciel EcoStruxure Power Commission.

Le logiciel EcoStruxure Power Commission est disponible sur www.se.com

Fonctionnalités clés

@TechPub Writer (10/2016): Variables used in the block “Key Features” are shared in maps D-SE-0059996 and D-SE-0052515.

EcoStruxure Power Commission software performs the following actions for the supported devices and modules:

  • Create projects by device discovery

  • Save the project in the EcoStruxure Power Commission cloud for reference

  • Upload settings to the device and download settings from the device

  • Compare the settings between the project and the device

  • Perform control actions in a secured way

  • Generate and print the device settings report

  • Perform a communication wiring test on the entire project and generate and print test report

  • View the communication architecture between the devices in a graphical representation

  • View the measurements, logs, and maintenance information

  • Export Waveform Capture on Trip Event (WFC)

  • View the status of device and IO module

  • View the alarm details

  • Buy, install, remove, or retrieve the Digital Modules

  • Check the system firmware compatibility status

  • Update to the latest device firmware

  • Perform force trip and automatic trip curve tests