MFR9435902-04

Overview

The section provides you information on viewing various parameter pages in the meter.

The meter navigation for DM6200H:

The meter navigation for EM1250H / EM1220H:

Information icons

Icons in the information area if the LCD display provides information such as what menu is selected.

Icon

Description

RMS

Energy and Non Reset Energy

Diagnostics

Old Energy

Reset

Setup

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?