MFR9435902-04

Power and Energy measurements

The meter lets you configure any one power parameter (W, VA, or VAR) at a time. You can set it using the meter’s display, through communication using ION Setup, or by any Modbus tool that supports FC16 (command number is 2959).

Energy accumulation in the meter depends on the selected power parameter (W, VA, or VAR). Integrated energy values, non reset energy and old values also depends on the selected power parameter.

NOTE:
  • On changing the power parameter (either through meter display or communication), all the stored energy values (old and integrated) are reset to zero.

  • Energy values can also be cleared through communication. Run Hours are displayed with 6 digit Hours and 2 Digit Minutes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?