MFR9435902-04

Favourite page

The meter allows you to select 3 parameters and arrange them in required order to be displayed in favourite page. These parameters can be selected only through communication and are based on your requirements. Some parameter logs are of utmost importance and navigating to those parameters takes time. For ease of navigation and accessibility, the meter allows you to lock the page for easy reading. The selectable parameters are:

  • V L-L

  • V L-N

  • A

  • F

  • W

  • PF

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?