MFR9435902-04

Meter Overview

The meters offers comprehensive 3-phase instrumentation and load management facilities in a compact and rugged package.

The meter is required to monitor an electrical installation which complies with Class 0.5 and Class 1.0 accuracy standards and feature high quality, reliability and affordability in a compact and easy to install.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?