MFR9435902-04

Reset screen menus

NOTE: Applicable for EM1250H and EM1220H.

Reset screen enables you to reset energy values. The meter’s display screen and buttons allow you to navigate and edit the required parameters.

To enter into reset parameters:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Reset.
  4. Press OK.
  5. Enter the password. Default password is 0000.
  6. Press OK.

The navigation of reset parameters:

Parameters Description

Energy

User can reset Energy parameters

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?