MFR9435902-04

Non reset energy page

NOTE: Applicable for EM1250H and EM1220H.

The parameters are available through communication and display in Maintain and cannot be reset. The values will overflow automatically when they reach maximum value.

To view Non Reset parameters:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Press the Up or Down button to navigate to the Non Reset Energy page.
  4. Press OK.
  5. Press the Up or Down button to navigate to the next Non Reset Energy parameter.
  6. Press Left button to exit.

The navigation of Non Reset Energy parameters:

EM1250H

Name on display

Description

KWh

Active energy

KVARh

Reactive energy

KVAh

Apparent energy

Rh

Run hours

EM1220H

Name on display

Description

KWh

Active energy

Rh

Run hours

The status of Non Reset Energy with the commands

Command Non Reset Energy

Reset sub systems

No clear (update with Accumulated energy)

Initialization

No clear (update with Accumulated energy)

Reset all accumulated energies

No clear (update with Accumulated energy)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?