MFR9435902-04

Editing setup parameters

The following steps describe how to edit parameters in setup mode:
  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Press the Up or Down button to navigate to Setup.
  4. Press OK.
  5. Enter password. Default password is 0000.
  6. Press OK.
  7. Press the Up or Down button to select a parameter to edit.
  8. Press OK button.
  9. Increase or decrease the digit value or select a value from a pre-programmed list using the Up or Down button.
  10. Press OK after making the required changes.
  11. Press Left button.
  12. Select Yes to save your settings.
    Done message displays.
NOTE: Select No to exit setup mode without saving any settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?