MFR9435902-04

Setup parameters

Name on display

Description

Input range

Default value

Basic Setup

Power System

Power System Configurations

[1PH2W LN, 1PH2W LL, 1PH3W LL, 3PH3W Dlt, 3PH4W Wye]

3PH4W Wye

VT Connect

Voltage Transformer [Direct Con, 2.VT, 3.VT, 1.VT]
NOTE: The VT Connect parameters are enabled based on selected power system configuration.
Direct Con

VT Primary(V)

Primary Voltage (V L-L) [100 V - 999000 V]
NOTE: VT.Primary(V) is not enabled if VT Connect is Direct Con.
415

VT Sec(V)

Secondary Voltage (V L-L) [100, 110, 115, 120, 415]
NOTE: VT.Sec(V) is not enabled if VT Connect is Direct Con.
415

CT on Term

Current Transformer [A.1, A.2, A.3, A.12, A.23, A.31, A.123]
NOTE: The CT on Term parameters are enabled based on the selected power system and VT connect configuration.
A.123

CT Primary(A)

CT Primary [1 A - 32767 A] 100

CT Sec(A)

CT Secondary [1 A, 5 A] 5

Sys Freq(Hz)

System Frequency [50 Hz, 60 Hz] 50

A.Suppress

A.Suppression (Minimum current at which meter starts functioning) [5 - 99 mA] 5

Label

Phase labeling [123, ABC, RST, PQR, RYB] 123

Full Scale%

Full scale value (Rescaling CT loading) [1 - 100] 100

Param Select

Parameter selection [VA, W, VAR] W

Poles

To determine RPM of alternator / generator based on number of poles and network frequency [02, 04, 06, 08, 10, 12, 14, 16] 04
LED Setup

LED Mode

LED parameter [OFF, Energy]
NOTE: Pulses/(k_h) is enabled when LED Mode is Energy of [1 to 9999000]
OFF
Communication Setup

COMM

Communication
  • ON / OFF: To enable / disable communications port.

  • Retrofit : For configuring legacy communication data models.

[ON, OFF, Retrofit,] ON

Address

Unit ID [1-247] 1

Baud Rate

BPS (Baud rate per second) [4800, 9600, 19200, 38400] 19200

Parity

Parity [Even, Odd, None] Even
HMI Setup

Contrast

Contrast [0 - 9] 5

Bcklght T.Out

Backlight time out [0 - 60] 5

Password

Password [0000 - 9999] 0000
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?