MFR9435902-04

Maintain page

The meter provides diagnostics information, old energy, non reset energy, reset and setup menus.

To view Maintain parameters:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next Maintain parameter.
  4. Press Left button to exit.
The navigation of Maintain page:

EM1220H / EM1250H

Name on display

Description

Diagnostics

You can view diagnostics parameters of the meter

Non Reset Energy

You can view non reset energy parameters

Old Energy

You can view old energy parameters

Reset

You can reset parameters

setup

You can view and edit setup parameters

DM6200H

Name on display

Description

Diagnostics

You can view diagnostics parameters of the meter

setup

You can view and edit setup parameters

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?