MFR9435902-04

Old energy page

NOTE: Applicable for EM1250H and EM1220H.
The parameters are available in communication and on meter display in Maintain page, which stores the accumulated energy of latest reset or overflow.

To view Old Energy parameters:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Press the Up or Down button to navigate to Old Energy page.
  4. Press OK.
  5. Press the Up or Down button to navigate to the next Old Energy parameter.
  6. Press Left button to exit.

The navigation of Old Energy parameters:

EM1250H

Name on display

Description

KWh

Active energy

KVARh

Reactive energy

KVAh

Apparent energy

Rh

Run hours

EM1220H

Name on display

Description

KWh

Active energy

Rh

Run hours

The status of Old Energy with the commands

Command Old energies

Reset sub systems

Clear

Initialization

Clear

Reset all accumulated energies

No clear (update with Accumulated energies)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?