Meter types
Meter model : DM6220H |
|
---|---|
Commercial reference | Description |
METSEDM6220HCL1 |
Class 1 panel mount meter, RS-485 and integrated display |
METSEDM6220HCL1LVD |
Class 1 panel mount meter with low voltage DC, RS-485 and integrated display |
Meter model : EM1220H |
|
Commercial reference |
Description |
METSEEM1220HCL1 |
Class 1 panel mount meter, RS-485 and integrated display |
METSEEM1220HCL5 |
Class 0.5 panel mount meter, RS-485 and integrated display |
METSEEM1220HCL5LVD |
Class 0.5 panel mount meter with low voltage DC, RS-485 and integrated display |
Meter model : EM1250H |
|
Commercial reference |
Description |
METSEEM1250HCL1 |
Class 1 panel mount meter, RS-485 and integrated display |