MFR9435902-04

RMS page

The meter provides highly accurate 1-second measurements, average values, including true RMS, per phase and total.

To view RMS parameters:

  1. From the Home (RMS) page, use Right / OK button to navigate to RMS.
  2. Press the Up or Down button to navigate to the next RMS parameter.
  3. Press Left button to exit.

The navigation of RMS parameters:

DM6220H

EM1250H

EM1220H

The list of RMS parameters are as follows:

  • Per-phase and average voltage (line-to-line, line-to-neutral)

  • Per-phase and average current, and neutral current (calculated)

  • Per-phase and average power factor

  • Per-phase and total power (VA, W, VAR)

  • System frequency

  • Revolutions per minute (RPM)

  • Unbalance (voltage, current)

  • Per phase load percentage

  • Per phase angle (between voltage and current)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?