MFR9435902-04

Comm(Communication) setup

Communication setup enables you to configure communication, address, baud rate, and parity parameters.

The meter’s display screen and buttons allow you to navigate and edit the required parameters.

To enter into Comm Setup:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Setup.
  4. Press OK.
  5. Enter the password. Default password is 0000.
  6. Use Up or Down button to navigate to Comm Setup.
  7. Press OK to enter Comm Setup.
  8. Press Left button to exit Comm Setup.
The navigation of Communication setup:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?