Energy page
The EM1220H meter provides uni-directional, Class 0.5 / Class 1 accurate energy metering.
The meter stores accumulated value of any one of the selected energy from active(kWh), reactive(kVARh) and apparent(kVAh) energy in non-volatile memory:
-
Delivered: kWh, kVARh, kVAh
The EM1250H meter provides uni-directional, Class 1 accurate energy metering.
The meter stores accumulated value of any one of the selected energy from active(kWh), reactive(kVARh) and apparent(kVAh) energy in non-volatile memory:
-
Delivered: kWh, kVARh, kVAh
To view Energy parameters:
- From the Home page, use Up or Down button to navigate to Energy.
- Press OK.
- Press the Up or Down button to navigate to the next Energy parameter.
- Press Left button to exit.
The navigation of energy parameter:
Name on display |
Description |
---|---|
KWh |
Active energy |
Rh |
Run hours |
Name on display |
Description |
---|---|
KWh |
Active energy |
KVARh |
Reactive energy |
KVAh |
Apparent energy |
Rh |
Run hours |
The status of energy with the commands:
Command | Accumulated energies |
Reset sub systems |
Clear |
Initialization |
Clear |
Reset all energies |
Clear |
Reset all accumulated energies |
Clear |