MFR9435902-04

Smart keys

The meter has four smart keys to navigate through the display pages. The display shows where you are headed.

Smart keys description

Right key / OK key
  • Going forward into sub-parameter pages.

  • To enter into Setup page. This action requires password.

  • Selecting the parameter to edit under Setup.

Left key
  • Going back to the main parameter pages.

  • Selecting previous digit on the left, under setup.

  • Exiting from editing Setup page.

Up key
  • Scrolling up through display pages at the same level, within the same function.

  • Increasing the value of the selected digit or navigating to the next available selection.

Down key
  • Scrolling down through other display pages at the same level, through all functions.

  • Decreasing the value of the selected digit or navigating to the next available selection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?