990-6401C-012

Dissipation thermique

  10 kVA 15 kVA 20 kVA 30 kVA 40 kVA
Mode normal (W) 700 1 050 1 400 2 100 2 800
Mode batterie (W) 750 1 125 1 500 2 250 3 000
Mode ECO (W) 200 300 400 600 800
Commentaires
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.