Alarm Thresholds
CAUTION |
|---|
|
Incorrect Alarm Settings
Do not change the alarm or warning thresholds unless the
battery setup changes. The alarm thresholds are set during the design
and configuration for each specific battery setup.
Failure to follow these instructions can result in injury or equipment damage.
|
To change the alarm threshold values:
-
Navigate to Devices > BACS > Alarm Thresholds from the side menu.
-
Here it is possible to change the different alarm thresholds and other settings for each type of alarm/warning:
-
Impedance
-
Voltage
NOTE: It is possible to set a delay for the voltage alarm. -
Temperature
-
-
Click Apply to confirm any changes.
NOTE: A new login might be required for the update to take effect.
CAUTION