0000509775_02_en

Module Ports, LEDs and Buttons

Part Name Description/Status
(A) Operation mode status LED Depending on the color and flashing speed the module is in different modes:
  • Green: Operation mode (address is programmed and communication is active).
  • Flashing green: Ready mode (address is programmed but communication is not active).
  • Alternating green and red: Search mode.
  • Red: Alarm mode (measurements are above or below the set threshold).
  • Flashing red: Default mode (no programmed address, default delivery state or after address reset).
  • Fast flashing red: Programming mode (address programming in progress, ready to be registered).
  • Off: Sleep mode (connected to the measuring cable but communication is not active).
(B) BACS bus ports Two RJ10 ports for bus connection.
(C) Address registration button Used to register a module when programming the address range of the setup. Can be pressed with the special accessory pen.
(D) Measurement cable port One port for the battery measurement cable connection.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?