0000509775_02_en

Network Settings

IMPORTANT: Make sure that the network settings confirm to your cyber security policy.

To change the network settings:

  1. Navigate to System > Network from the side menu.

  2. Here it is possible to specify a static IP address and network settings for the webmanager. It also shows the MAC address and the current active network settings.

  3. Click Apply to confirm any changes.

    NOTE: A new login might be required for the update to take effect.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.