0000509775_02_en

Prepare the Batteries

Before you attach the EcoStruxure Battery Management System module fastening strips, check that the battery surface is clean and dry. To clean the battery surface:

  1. Check what cleaning product is recommended by the battery manufacturer.

    NOTE: If you are unsure or there are no recommendations available use only soapy water.

  2. Clean the surface of the batteries with the recommended cleaning product.

  3. Dry the surface of the batteries with an antistatic fabric.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.