0000509775_02_en

Language Settings

To change the language viewed in the web interface:

  1. Navigate to System > General from the side menu.

  2. Under the Region section it is possible to change the displayed language and temperature format.

  3. Click Apply to confirm the change.

    NOTE: A new login might be required for the update to take effect.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?