DOCA0184EN-07

Circuit Breaker and Switch Disconnector Favorite

The circuit breakers, switch disconnectors and residual current circuit-breaker selected as favorite product are sorted by switchboard type (main panel or subpanel).

A reminder is located on the top of the diagram view at the left side to precise the type of the switchboard which is being configurated by the user.

If the user wants, under his responsibility, to use one of these favorites in a different switchboard type, he can access to it by clicking all on the favorites role filter.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.