DOCA0184EN-07

Select and Mount the Distribution and Mechanical Elements

To open the distribution block selector, click the Distributions & FUsbutton > DISTRIBUTIONS.

It is possible to directly select a distribution block range by clicking the range picture and validate.

Choose the range and configure the features of the distribution block you selected, and then validate them.

From the workbench, drag and drop the distribution block in the enclosure (this drag and drop function is not available for comb busbar range)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.