DOCA0184EN-07

Switchboards View

The list view is dedicated to the creation of the switchboard(s) of the project, the graphic view is dedicated to the connection between the different switchboards (including already existing switchboards in the installation if necessary).
  • Compulsory data for each panel:

    • Name of the panel.

    • Position of the panel in the installation: main panel or sub panel.

    • Number of phases at the incoming of the panel.

  • Optional panel data:

    • Short circuit current value at the incoming of the panel.

    • Incoming current value in the panel.

Click the Create button of a panel in the list to open the Diagram page of the panel.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.