DOCA0184EN-07

Print preview

This preview allows to visualize the number of printed pages regarding the SLD. This number of pages can be optimized according to the number of columns/devices displayed per page and the level of readability requested. The +/- zoom function allows to set up the number of pages.

You can see the downstream multiple circuits diagram in the places where you have added the card in Diagram.

The single line diagram can be generated in .pdf format by clicking the Export button; it is also accessible from the Documents page.

The generated pdf document has a header page with:

  • The logo and company data (if uploaded in the user account)

  • The project information as well as the table information (mandatory and optional data)

  • An insert is reserved for the management of versions and related modifications. Each following page includes, in addition to the elements of the one-line diagram, a footer with the logo of the user's company, the name of the project, the creation date.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.