DOCA0184EN-07

Electrical Diagram Structure and Principle of Use

The main incomer role card of the electrical diagram is already in place.

The main incomer role card cannot be removed from the electrical diagram but can be substituted by the transfer switch card if needed.

The electrical diagram is built by adding role cards out of a list. The list of role cards is accessible in the foldable section on the left side of the page:

  • Residual current relay

  • Group feeder

  • Outgoer

  • Residual current circuit breaker

  • Load circuit control

  • Scheduling-Management

  • Energy meter

  • Switch disconnector

  • Miscellaneous

  • Signalisation

  • Multiple circuits

  • Transfer switch

  • Generator protection

For each role card in the electrical diagram, the user shall choose a product range or a product in the proposed selection of Schneider Electric catalogue before moving to the next steps in the application.

The Downstream multiple circuits role card is used downstream an outgoer role card to display the corresponding line in the single line diagram and does not propose any product range.

Any change to the electrical diagram and in the products selection in a panel can be done from the Diagram page of this panel.

No change is possible from any other page of the application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.