DOCA0184EN-07

Front View

The list of the panels in the project is accessible from the electrical diagram and single line diagram page.

To switch to another panel in the project:

  • Click on the name of the panel which is currently displayed.

  • Click on the name of another panel in the list.

Click to undo any operation.

Click to redo any operation.

NOTE: You can undo and redo up to 10 steps.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.