DOCA0184EN-07

Navigate in the Electrical Diagram

To navigate in the electrical diagram:

  • Handle the electrical diagram wherever possible (for example, empty space) and move it in all directions.

  • Use the mini map bottom-right to figure out which part of the electrical diagram is displayed.

  • Handle and move the blue rectangle in the mini map to navigate into the electrical diagram.

To zoom in and zoom out the electrical diagram:

  • Use the scroll wheel of the mouse or two fingers on the computer pad.

  • Click the magnifying glass icon at the top of the page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.