DOCA0184EN-04

Create Snapshot of the Panel Front View

It is possible to create a snapshot of the displayed front view of the panel by clicking the camera icon on the top bar of the screen. The snapshot is saved on the computer and can be added to the project documentation (refer Documents).

The snapshot of the panel is included in the project report document.

QR code for this page

Was this helpful?