DOCA0184EN-07

Project Information View

This page allows you to create the project and to manage the project description:

  • Compulsory data for each project: name of project.

  • Optional project data: list of contacts for the project with several information to enter for each contact.

  • These data are displayed on the first page of the project report which can be accessed from Documents page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.